Application Common Services
Digital App Center
The dashboards and the application build are deployed using the Digital Apps Center (DAC). Following are the features in
Genix Suite 25.2
In-App Help
When you click
in Digital Application Center, it opens the help documentation for the activity you are currently performing.
The help documentation opens as a sidepanel so you do not have to switch between windows. You can click
icon to open the help documentation in a new tab. Click
to close the sidebar. You can also search for the required document using
icon.
Language Support
This allows users to interact with the UI in their preferred language and makes it more user-friendly, leading to improved satisfaction. You can select one of the following as a preferred language for your applications:
-
Chinese (Simplified)
-
English
-
Portuguese
-
Spanish
-
Swedish
If an application does not support the selected language, all information present under that application will be displayed in English by default.